Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the difference between A type and B type LCD drive timing?

Latest Updated:10/19/2004

Question:

(LCD)  What is the difference between "A type" and "B type" LCD drive timing ? [2004/10/19]

Answer:

A type is equivalent to existing Renesas products.
B type can support LCD panels of slow responsivity.
Please select which type to use according to your LCD panel. (#104921)
Suitable Products
38D2