What is the characteristics of enhancement type of MOS FET?
Latest Updated:11/01/2005
Question:
What is the characteristics of enhancement type of MOS FET?
Answer:
This is a type of MOS FET. An enhancement type MOS FET has a characteristic that a drain current does not flow unless a gate voltage is applied. The gate voltage at which the drain current starts flowing is specified as a threshold voltage VT.
Today, enhancement type MOS FETs are generally used.
Today, enhancement type MOS FETs are generally used.

Suitable Products