What is the A/D conversion speed?
Latest Updated:02/14/2006
Question:
What is the A/D conversion speed?
Answer:
It is:
33 øAD cycles in 10-bit resolution with a sample & hold;
28 øAD cycles in 8-bit resolution with a sample & hold.
For example, it is 2.06µs for M32C/85 Group (øAD=16MHz, 10-bit resolution with a sample & hold) and 2.75µs for M16C/62P Group (øAD=12MHz, 10-bit resolution with a sample & hold).
33 øAD cycles in 10-bit resolution with a sample & hold;
28 øAD cycles in 8-bit resolution with a sample & hold.
For example, it is 2.06µs for M32C/85 Group (øAD=16MHz, 10-bit resolution with a sample & hold) and 2.75µs for M16C/62P Group (øAD=12MHz, 10-bit resolution with a sample & hold).
Suitable Products
M32C/8A |
M32C/88 |
M32C/87 |
M32C/85 |
M32C/84 |
M32C/83 |
M32C/80 |
M16C/62A |
M16C/62A(M16C/62T) |
M16C/62M |
M16C/62N |
M16C/62N(M3062GF8NFP, M3062GF8NGP) |
M16C/62P |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |
M16C/1N |