Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is difference between the H8/3664 and the H8/3694 groups?

Latest Updated:03/24/2009

Question:

What is difference between the H8/3664 and the H8/3694 groups?

Answer:

These groups have the same integrated functions and pin arrangement, except for the following point ;
1. The operating frequency is leveled up to 2 to 20MHz/4.0 to 5.5V for H8/3694 while 2 to 16MHz/4.0 to 5.5V for H8/3664. 
2. For H8/3694, the IIC bus I/F module is improved for easy-to-use. 
3. Power-on reset function (POR) and low power detection function (LVD) are provided as option in H8/3694.
Suitable Products
H8/300H Tiny
H8/3694
H8/3664