Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is correct: data written on SOTB1 side or dummy in reception side

Latest Updated: 03/22/2017

Question:

After setting "transmit/receive mode" on both sides, when transmit data is written to SOTB1 on the transmitting side, it is still in the transfer wait state and when dummy data is written from the reception side to SOTB1 under these conditions, then data will be transferred. Is this correct?

Answer:

No.
Transmission starts when the master, the transmitting side, writes transmit data to SOTB1.
Here, data transfer starts regardless of the state of the receiving side.

On the other hand, if transfer start has not been set on the receiving side (in the case of transmit/receive mode, dummy data has not been written to SOTB), the receiving side ignores the serial clocks, however many are sent.

That is, the master must start the transfer after transfer start has been set on the slave side.
If this order is not observed, normal transfer cannot be executed.

Suitable Products
V850 Family