Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is Internal Power Supply Generator (VDC)?

Latest Updated:09/10/2007

Question:

What is Internal Power Supply Generator (VDC)?

Answer:

Internal Power Supply Generator (VDC) is a function that converts 5V and 3.3V, which are input to VCCER (main power supply) pin, to the voltage level for internal use.
Suitable Products
32185
32186
32192
32195
32196
  • Este artigo foi útil?