What is Clock skew?
Latest Updated:08/01/2005
Question:
What is Clock skew?
Answer:
When multiple circuits are synchronized with a clock, a clock delay is generated and the setup time and hold time cannot be satisfied if there is a critical path that extends routing of the clock line or a gate clock with a logic gate installed on the clock line.
Consequently, the clock cannot sample data in the correct timing. This phenomenon is called clock skew.
Consequently, the clock cannot sample data in the correct timing. This phenomenon is called clock skew.

Suitable Products