What happens if 0 is written in A/D converter completion bit when it is 0?
Latest Updated:03/01/2005
Question:
(A/D Converter) What happens if "0" is written to the A/D converter completion bit when the bit is "0" (conversion in progess) ? [2005/03/01]
Answer:
If "0" is written to the A/D converter completion bit while the bit is "0" (conversion in progess), conversion will restart from the beginning. (#104832)
Suitable Products
3803H |
3803L |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7546 |
7547 |
7548 |
7549 |