Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Should data be set from b15 or b0 when using SSU to perform 9-15 bit data transfer?

Last Updated:12/26/2017

Question:

When using the synchronous serial communication unit (SSU) to perform 9- to 15-bit data transfer, should the data be allocated from b15, or b0?

Answer:

Allocate the data from b0. Write 2FFh in 16-bit units when transmitting 2FFH (10-bit data).
Suitable Products
R8C/3x
R8C/5x
R8C/Lx
R8C/Mx