Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

ROMless / Mask ROM versions: is this a dedicated WDTOVF# terminal?

Latest Updated:01/18/2008

Question:

In the manual, there's a combination WDTOVF#(FEW,EMLE) terminal; in the ROMless/Mask ROM versions, is this a dedicated WDTOVF# terminal?

Answer:

Yes, in the ROMless/Mask ROM versions it is a dedicated WDTOVF# terminal.
Suitable Products
H8S/2398, 2357
H8S/2345
H8S/2329
H8S/2319