Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Meaning of td(P-R)

Latest Updated:10/05/2016

Question:

What is the meaning of "time for internal power supply stabilization during power-on" (td(P-R)) in electrical characteristics?

Answer:

td(P-R) is the time that it takes for the internal power supply generating circuit to stabilize after the power supply is turned on.
For example, if td(P-R) is max. 2000 us, this means that if at least 2000 us have elapsed after the power supply has been turned on, the internal power supply generating circuit has stabilized.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/33T
R8C/3JT
R8C/3NT
R8C/36T-A
R8C/38T-A
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A
R8C/Mx