Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there anything I need to do regarding the interrupt processing?

Latest Updated:01/18/2008

Question:

I'm using a product with a subclock. After directly transistioning between high-speed mode and subactive mode, direct transistion interrupt processing starts. Is there anything I need to do regarding the interrupt processing? (Are functions possible without the processing?)

Answer:

No register setting changes, etc. are necessary, but don't forget RTE instructions for returning from exception handling routines.
Suitable Products
H8S/2649
H8S/2648, 2646
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2615
H8S/2282, 2280
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2214
H8S/2218, 2212
H8S/2189R
H8S/2168
H8S/2148, 2144
H8S/2144B,2134B
H8S/2140B
H8S/2138, 2134
H8S/2125
H8S/2128, 2124
H8S/2117, 2117R
H8S/2116
H8S/2114R
H8S/2111B
H8S/2110B