Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there any product in Lead-Free package?

Latest Updated:03/25/2009

Question:

Is there any product in Lead-Free package?

Answer:

Yes, we have Lead-Free products which is specified by the code “V” added to the end of product name.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902