Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there any caution when using bit manipulation instruction?

Latest Updated:03/26/2009

Question:

Is there any caution when using bit manipulation instruction?

Answer:

Users are advised to exert caution when using the register with write-only bits. For detail explanation, please refer section "Bit Manipulation Instruction" in the hardware manual.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902