Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is there a chance that interrupt request becomes 1 if change using INT?

Latest Updated:06/11/2012

Question:

When the interrupt priority level select bit and polarity select bit are changed when using INT interrupts, is there a possibilty that the interrupt request bit becomes "1"?

Answer:

The interrupt request bit does not become "1" when the interrupt priority level select bit is changed. However, there is a possibility it may become "1" when the polarity select bit is changed. Therefore, when the polarity select bit is changed, you need to clear the interrupt request bit to "0".
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N