Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is the value of TCWE held 0 when it is written in the status of TCSRWD?

Latest Updated:03/18/2009

Question:

When using the watchdog timer on the Tiny series when 1 is written to the timer counter W writing enable (TCWE) bit of the timer control /status register (TCSRWD) is the value 1 held until the next 0 is written ?

Answer:

Yes 1 is held until the next 0 is written.
Suitable Products
H8/300H Tiny