Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is setting made with PCR when using SCI? How is the input for SCK chosen?

Latest Updated:03/25/2009

Question:

When using SCI, how is the input for SCK selected? Is this setting made with the port control register (PCR)?

Answer:

When using SCI, the selection of the SCK pin function is made with COM bit of the serial mode register (SMR) and CKE1 and CKE0 of the serial control register (SCR). It is not necessary to set the PCR.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power