Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is receive clock generated at fall of start bit and does delays occur?

Latest Updated:03/01/2005

Question:

(Serial Interface)  Is the UART receive clock generated at the fall of the start bit? During a continuous receive, does a gradual delay of the receive clock occur? [2005/03/01]

Answer:

The receive clock is generated at the fall of the start bit. Consequently, a gradual delay of the receive clock does not occur during a continuous receive. (#104802)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549