Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is output level undefined if counter stops output mode of Timer A?

Latest Updated:02/27/2012

Question:

When the counter stops after outputting the pulse in the pulse output mode of Timer A, is the output level undefined ?

Answer:

It depends on the mode of Timer A.

  • In Timer Mode:
    It outputs "L" during counter stop.
  • In Event Counter Mode:
    It outputs "L" during counter stop.
  • In One-shot Timer Mode:
    It outputs "L" during counter stop.
    It outputs "H" during count.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/24 (M30245)
M16C/29
M16C/28
M16C/26A