Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is it possible to exit software standby mode for IRQ2 1 0 by setting ISCR?

Latest Updated:03/23/2009

Question:

Is it possible to exit software standby mode for IRQ2,1,0 choosing any of the following, *Low level, *Rising edge, *Falling edge, *Both falling and rising edge, by setting the ISCR ?

Answer:

Yes, it is possible to exit software standby mode with any of the settings.
Suitable Products
H8S/2345