Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is it needed to set flash memory control register to program serial?

Latest Updated:10/19/2004

Question:

(Flash Memory)   When programming using a serial programmer, is it necessary to set the flash memory control register? [2004/10/19]

Answer:

It is not necessary to set the flash memory control register. (#104912)
Suitable Products
3803H
3803L
3850A
38D2
38D5