Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is changes needed to the program if replacing device with ROM version?

Latest Updated:08/01/2001

Question:

During development using the flash version of the uPD78F9177Y, when replacing the device with the mask ROM version, do I need to make modifications to the program?

Answer:

There is no particular need for modifications.
In the case of assembly, create the program file using the uPD789177Y device file, and then check its operation with the flash version.
Suitable Products