Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Is an internal pull up resister enabled on the setting using XIN port?

Latest Updated:12/06/2013

Question:

When using the port as the XIN clock pin (pins XIN and XOUT), or XCIN clock pin (pins XCIN, XCOUT), is an internal pull-up resister enabled depending on the setting?

Answer:

An internal pull-up resister is disabled regardless of setting.
Suitable Products
R8C Family