Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

In what way does the receive-action differ in continuous receive mode?

Latest Updated:09/22/2010

Question:

In what way does the receive-action differ when the continuous receive mode is or is not selected?

Answer:

In clock synchronous serial I/O mode, writing dummy data to the transmit buffer register starts output from the transmit/receive clock. Therefore, even when only receiving, it is necessary to read the receive buffer register and write dummy data to the transmit buffer register.
However, when continuous receive mode is selected, the transmit/receive clock output starts when data is read from the receive buffer register. Therefore, it is not necessary to write dummy data to the transmit buffer register in this case (do not write dummy data).
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N