Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

In what situation is the bus collision detection function used?

Latest Updated:01/09/2009

Question:

(Serial Interface)  In what situation is the bus collision detection function used? [2009/01/09]

Answer:

The bus collision detection must be used when more than one MCU is operating at full-duplex communication, and the RxD and TxD pins of all the MCUs are connected to a single bus line.

For information on using the bus collision detection function, please refer to the application notes. → here
(#107247)

Suitable Products
7546
7547