Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to set up output from port if PFO is selected by FSR?

Latest Updated:02/14/2006

Question:

How should I set to output from a port, when Peripheral Function Output is selected by Function Select Register?

Answer:

Please switch to the I/O port by Function Select Register after setting to the output port by Direction Register and the level by Port Register.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80