Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to put I2C bus interface slave reception into wait state

Latest Updated:10/05/2016

Question:

How do I put the slave reception operation of the I2C bus interface into a wait state?

Answer:

If the RDRF bit is 1, a wait state is automatically entered (SCL becomes low level) at the fall of the eighth clock of SCL. To exit the wait state, read the ICDRR register.
Suitable Products
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32M
R8C/33M
R8C/34M
R8C/35M
R8C/36M
R8C/38M
R8C/3GM
R8C/3JM
R8C/3MK
R8C/34K
R8C/3MU
R8C/34U
R8C/3MQ
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
R8C/L35M
R8C/L36M
R8C/L38M
R8C/L3AM
R8C/LA3A
R8C/LA5A
R8C/LA6A
R8C/LA8A