Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to properly write the address in C source?

Latest Updated:04/01/2006

Question:

Because I described all interrupts in C, I wrote the addresses to be registered to the vector table using the assembler and set the jump destination to the same place as the reset status.
I believe these are all that must be described in the C source; is there a problem with it?

Answer:

With this processing, once the watchdog timer interrupt occurs, interrupts will subsequently be unable to be acknowledged.
In this case, make a setting to ensure that a reset occurs when the watchdog timer overflows.
Suitable Products
78K Family