Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How to configure the registers associated with timer RC if not stable?

Latest Updated:12/06/2013

Question:

If the operating clock of timer RC is not stable, can I configure the registers associated with timer RC?

Answer:

Do not access the registers associated with timer RC when the operating clock is not stable. Same applies to timer RD, and timer RG.
Suitable Products
R8C/2x
R8C/3x
R8C/5x
R8C/Lx
R8C/Mx