Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How does the power consumption of the H8S compare with the H8/300H?

Latest Updated:03/18/2009

Question:

How does the power consumption of the H8S compare with the H8/300H ?

Answer:

In single chip mode the H8S current consumption is about 1/3 of the H8/300H for similar performance. However the clock gearing and module standby functions can improve this further.
Suitable Products
H8/300H
H8S Family