Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

How are I/O ports when move with no sub oscillator on H8/3802, H8/38024?

Latest Updated:03/18/2009

Question:

What is the condition of the I/O ports when the processor transfers to watch mode without the sub-oscillator being present on H8/3802 and H8/38024 series ?

Answer:

The port maintains the status it had immediately before the transfer for both input and output port. It is not recommended to transfer to the sub-clock type mode without connecting a sub-oscillator. If not connecting to any sub-oscillator be sure to fix X1 pin to GND.
Suitable Products
H8/300L Super Low Power
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3802, 38002S, 38004, 38104
H8/300L
H8 Super Low Power