H8/300H Tiny series: Any products with temperature of -40 to +85 °C
Latest Updated:03/25/2009
Question:
In the H8/300H Tiny series lineup, are there any products with an operating temperature range of -40 to +85 degrees Celsius?
Answer:
Yes, there are products with an operating temperature range of -40 to +85 degrees Celsius in Tiny series. If you want to purchase them, please contact to our local sales or distributors for their availability.
Suitable Products
H8/300H Tiny |
H8/36109 |
H8/36087 |
H8/36077, H8/36079 |
H8/36064 |
H8/36049 |
H8/36037, H8/36057 |
H8/36014, H8/36024 |
H8/3694 |
H8/3687 |
H8/3672 |
H8/3664 |
H8/36912, H8/36902 |