Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Do I need to erase ID in Mask ROM when replacing the Flash Memory Version?

Latest Updated:02/27/2012

Question:

ID is written to the stored addresses of ID code in order to use ID code check function in the Flash Memory Version. When replacing to the Mask ROM Version from the Flash Memory Version, do I need to erase this ID in the Mask ROM Version?

Answer:

No, you do not need to erase it.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N