Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can you explain the relationship between writing timing and waveform?

Latest Updated:03/26/2009

Question:

The application note, "14-Bit PWM Function Based Variable Duty-Cycle Pulse Output" states that there may be occasions when a normal PWM waveform will fail to be output due to the timing needed to overwrite the PWM data register. Please explain the relationship between writing timing and waveform.

Answer:

Standard pulses are formed by the use of a counter in the PMW wave-forming section, in other words, by securing compare match between the value of the counter (TCNT) and the value of the compare match register corresponding to the standard pulse width. In some cases, rewriting the PWM register may generate abnormal waveforms, because the value of compare match register is changed during operation.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902