Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can we transfer first MSB to LSB to register smart card interface?

Latest Updated:03/31/2009

Question:

Will the serial interface data be transferred in order from MSB-first to LSB when selecting MSB-first transmit in the SCMR register in smart card interface?

Answer:

Yes, it will. The LSB/MSB-first function of smart card interface is directly usable in the serial interface.

*Note: H8/300H only.

Suitable Products
H8 Family
H8/300H
H8/3069R
H8/3068
H8/3067(H8/3065, H8/3066, H8/3067)
H8/3062(H8/3060, H8/3061, H8/3062)
H8/3052B
H8/3048B
H8/3048(H8/3044, H8/3045, H8/3047, H8/3048)
H8/3042(H8/3040, H8/3041, H8/3042)
H8/3039(H8/3036, H8/3037, H8/3038, H8/3039)
H8/3035(H8/3033, H8/3034, H8/3035)
H8/3032(H8/3030, H8/3031, H8/3032)
H8/3029F
H8/3029
H8/3028(H8/3028, H8/3028F)
H8/3024(H8/3024, H8/3026)
H8/3022(H8/3020, H8/3021, H8/3022)
H8/3008
H8/3006(H8/3006, H8/3007)
H8/3004(H8/3004, H8/3005)
H8/3003
H8/3002
H8/3001