Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can the voltage drop detection circuit be used during RC oscillation?

Latest Updated:07/04/2003

Question:

(Low Voltage Detection/LVD)   Can the voltage drop detection circuit be used during RC oscillation?

Answer:

Yes. The voltage drop detection circuit is not dependent on the state of oscillation. (#105017)
Suitable Products
4559