Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can the counter be restarted by the count enable?

Latest Updated:10/19/2004

Question:

When using the TIO Timer in "noise processing input mode", although an effective level signal continues to be input from an external TIN pin, counting is stopped by under flow of the counter. Can the counter be restarted by the count enable? Moreover, what is the value of the counter at the time of the restart if the counter enable can restart?

Answer:

Yes, the counter can be restarted by count enable.

The counter restarts from the value that has been set in the reload register upon count enable restart while the input signal at the external TIN pin remains asserted.

Suitable Products
32170, 32174
32171
32172, 32173
32176
32180
32182
32185
32186
32192
32195
32196