Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can the VPP pin be connected to VSS via pull-down resistor?

Latest Updated:12/01/2011

Question:

When using the flash version of the uPD78F9418A, the VPP pin must be connected to VSS when it is not used; but is it necessary to connect it directly to VSS?
Can the VPP pin be connected to VSS via a pull-down resistor (several kΩ to several tens of kΩ)?

Answer:

No, VPP does not have to be connected directly to VSS.
It can be connected to VSS via a pull-down resistor of approximately 10kΩ.
However, in this case malfunction may occur due to system noise, so the customer should evaluate this carefully.
Suitable Products
UPD1793xx
UPD7800xx
UPD7803xx
UPD7807xx
UPD7808xx
UPD7809xx
UPD780xx
UPD7890xx/7891xx
UPD78902x
UPD7893xx/7894xx
UPD7898xx
UPD784xxx