Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can SCI and IIC used simultaneously despite same address allocation?

Latest Updated:01/18/2008

Question:

The SCI register and IIC register have the same address allocation. Can SCI and IIC be used simultaneously?

Answer:

Simultaneous use of SCI and IIC is not possible for the H8S/2633 and H8S/2634 groups. Simultaneous use of SCI and IIC is possible for other products. When using, please set the SCI SMR, BRR, SCMR registers first, then switch to the IIC ICCR, ICSR, ICDR/SARX registers.
Suitable Products
H8S/2643
H8S/2630, 2639, 2638, 2636, 2635
H8S/2633
H8S/2268, 2264
H8S/2258, 2239, 2238, 2237, 2227
H8S/2189R
H8S/2168
H8S/2148, 2144
H8S/2140B
H8S/2138, 2134
H8S/2125
H8S/2128, 2124
H8S/2117, 2117R
H8S/2116
H8S/2114R
H8S/2111B
H8S/2110B