Can I use any of the rising, falling or both edges as the INT polarity?
Latest Updated:02/14/2006
Question:
I want to use an INT interrupt (external input) to release the MCU from the stop mode. In this case, can I use any of the following as the INT interrupt polarity: rising edge, falling edge, or both edges?
Answer:
Any of the above can be used.
Suitable Products
R8C/18 |
R8C/19 |
R8C/1A |
R8C/1B |
R8C/20 |
R8C/21 |
R8C/22 |
R8C/23 |
R8C/24 |
R8C/25 |
R8C/26 |
R8C/27 |
R8C/28 |
R8C/29 |
R8C/2A |
R8C/2B |
R8C/2C |
R8C/2D |
R8C/2E |
R8C/2F |
R8C/2G |
R8C/2H |
R8C/2J |
R8C/2K |
R8C/2L |
R8C/32C |
R8C/33C |
R8C/34C |
R8C/35C |
R8C/36C |
R8C/38C |
R8C/3GC |
R8C/3JC |
R8C/32D |
R8C/33D |
R8C/35D |
R8C/3GD |
R8C/33T |
R8C/38A |
R8C/34E, R8C/34F, R8C/34G, R8C/34H |
R8C/36E, R8C/36F, R8C/36G, R8C/36H |
R8C/38E, R8C/38F, R8C/38G, R8C/38H |
R8C/L35C |
R8C/L36C |
R8C/L38C |
R8C/L3AC |
M32C/8A |
M32C/88 |
M32C/87 |
M32C/85 |
M32C/84 |
M32C/83 |
M32C/80 |
M16C/62A |
M16C/62A(M16C/62T) |
M16C/62M |
M16C/62N |
M16C/62N(M3062GF8NFP, M3062GF8NGP) |
M16C/62P |
M16C/63 |
M16C/64A |
M16C/64C |
M16C/65 |
M16C/65C |
M16C/6C |
M16C/6N4, M16C/6N5 |
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN |
M16C/5L, M16C/56 |
M16C/5LD, M16C/56D |
M16C/5M, M16C/57 |
M16C/30P |
M16C/29 |
M16C/28 |
M16C/26A |
M16C/1N |