Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Can I use H8S/2357 to accept DMAC request during internal operation?

Latest Updated:03/23/2009

Question:

Is it possible for the H8S/2357 to accept DMAC startup request during CPU internal operation?

Answer:

Its possible since the CPU releases the internal bus during its internal operation.
Suitable Products
H8S/2398, 2357