Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Av. output current: electrical characteristics in hardware manual

Latest Updated:01/11/2008

Question:

What is the average output current indicated for electrical characteristics listed in the hardware manual?

Answer:

The average output current is the average of the output current within a 100 ms period. Take the R8C/25 Group, for example. Port P2_0 must fill both conditions that the low peak output current is a maximum of 40 mA and the low average output current is a maximum of 20 mA. One example would be to output a 40 mA current for 50 ms, and output a second 0 mA current for 50 ms. The 20 mA average output current is achieved. This can also be achieved by outputting 20 mA continuously for 100 ms. However, the low average sum output current must be a maximum 80 mA.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC