Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

At which point can I switch the clock after oscillation has stabilized?

Latest Updated:02/14/2006

Question:

After the oscillation has stabilized, at what point can I switch/change the main clock division rate? Also, can I execute an instruction immediately after switching the clock division rate?

Answer:

Once the oscillation has completely stabilized, the main clock division rate can be switched at any time. In addition, yes, you can have an instruction immediately after the instruction that switches the division rate.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N