Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there products operate with the range of -40 to 85 degrees Celsius?

Latest Updated:03/25/2009

Question:

In the SLP product lineup, are there any products with an operating temperature range of -40 to 85 degrees Celsius?

Answer:

Yes, there are products with an operating temperature range of -40 to 85 degrees Celsius in SLP Microcomputer. If you want to purchase them, please contact to our local sales or distributors for its product availability.
Suitable Products
H8/300H Super Low Power
H8/38602R
H8/38086R
H8/38086
H8/38076R
H8/300L Super Low Power
H8/3887
H8/3867
H8/3857
H8/3854F
H8/3854
H8/38024R, 38024, 38024S, 38124
H8/38024F
H8/3824
H8/3802, 38002S, 38004, 38104
H8 Super Low Power