Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

Are there any Tiny devices with on-chip EEPROM ?

Latest Updated:03/18/2009

Question:

Are there any Tiny devices with on-chip EEPROM ?

Answer:

The H8/3664N uses Renesas Multi chip packaging capability to provide a pin compatible device to the H8/3664 with 512 bytes of on-chip EEPROM. This devices is available in both flash ( 32 kbytes on chip ) and a variety of mask ROM versions.
Suitable Products
H8/300H Tiny