Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

(H8S Family) What are the advantages and disadvantages of DMAC over DTC?

Latest Updated:03/18/2009

Question:

What are the advantages and disadvantages of DMAC over DTC ?

Answer:

Disadvantages : Cost / Limited number of channels / Limited number of trigger sources / Complexity. Advantages : Speed of transfer / Easier to configure.

Suitable Products
H8S Family