Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

(7544)Can external capacitor be used to regulate the density of oscillator?

Latest Updated:03/01/2005

Question:

(Clock)  Can an external capacitor or resistor be used to regulate the frequency of the on-chip oscillator ? [2005/03/01]

Answer:

No. The on-chip oscillator does not require an external capacitor or resistor. The frequency is determined by the power supply voltage and operating ambient temperature. (#104854)
Suitable Products
7544