Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

(3850A) In the QzROM, can additional programs be written to the free area in ROM?

Latest Updated:06/06/2007

Question:

(QzROM)  In the QzROM version, can additional programs be written to the free area in ROM ? [2007/06/06]

Answer:

As long as protect is not enabled, it is possible to write to the ROM.
However, be careful not to "overwrite" bits that have already been written to. (#106722)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549