Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

(3850A) How do you enable protection in the QzROM version?

Latest Updated:06/06/2007

Question:

(QzROM)  How do you enable protection in the QzROM version ? [2007/06/06]

Answer:

For QzROM programming using a programmer, set protection using the programmer. For the setting method, please refer to the programmer manual.
For products programmed and shipped by Renesas, set protection in the ROM options in the mask file converter (MM).
Please note enable/disable of the ROM code protect function cannot be set from source files or HEX files. (#106720)
Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7545
7546
7547
7548
7549