Pular para o conteúdo principal
Knowledgebase
Home
Renesas Brasil - Knowledgebase

What is the criteria by which PLP products are selected?

Latest Updated:04/01/2015

Question:

What is the criteria by which PLP products are selected?

Answer:

PLP products are selected based on the following criteria or conditions.
1. The product is published on the Renesas website (custom products and products developed for a specific restricted use, etc. are excluded)
2. Products for industrial and other applications that require long a product life cycle in general (automotive products are excluded, see FAQ No. 1010889)
3. The product meets the conditions set by Renesas
Suitable Products
PLP (Product Longevity Program)